Way to dicide a tRPA parameter settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Way to dicide a tRPA parameter settings

ソリューションへジャンプ
2,682件の閲覧回数
ko-hey
Senior Contributor II

Hi all

How to decide a tRPA parameter in script aid ?

I'm setting a i.MX6SL's DDR3 parameters and using following script aid.

i.MX6SL DDR3 Register Programming Aid

I can't find any description and data about tRPA in DDR3's datasheet and find only following description in i.MX6SL's reference manual.

But I can't understand which setting is suit for DDR3.

pastedImage_1.png

I also checked a DDR3 SDRAM Specification JESD79-3E (July 2010) but can't find any description about it.

I attached a DDR3's datasheet.

So could you point where it is in attached datasheet ?

Ko-hey

ラベル(2)
0 件の賞賛
返信
1 解決策
2,178件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  if the tRPA (PREA) is not provided in DRAM datasheet, one can

set it as tRP or  tRP+1 for assurance.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,179件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  if the tRPA (PREA) is not provided in DRAM datasheet, one can

set it as tRP or  tRP+1 for assurance.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,178件の閲覧回数
ko-hey
Senior Contributor II

Hello Yuri

I understand as follow.

User can set it whichever user like if it not describe in datasheet.

User need test both of parameters, right ?

Ko-hey

0 件の賞賛
返信
2,178件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, users can try both cases : tRPA = tRP and tRPA = tRP+1

~Yuri.

2,178件の閲覧回数
ko-hey
Senior Contributor II

OK, thanks.

Ko-hey

0 件の賞賛
返信