Way to dicide a tRPA parameter settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Way to dicide a tRPA parameter settings

Jump to solution
1,385 Views
ko-hey
Senior Contributor II

Hi all

How to decide a tRPA parameter in script aid ?

I'm setting a i.MX6SL's DDR3 parameters and using following script aid.

i.MX6SL DDR3 Register Programming Aid

I can't find any description and data about tRPA in DDR3's datasheet and find only following description in i.MX6SL's reference manual.

But I can't understand which setting is suit for DDR3.

pastedImage_1.png

I also checked a DDR3 SDRAM Specification JESD79-3E (July 2010) but can't find any description about it.

I attached a DDR3's datasheet.

So could you point where it is in attached datasheet ?

Ko-hey

Labels (2)
0 Kudos
Reply
1 Solution
881 Views
Yuri
NXP Employee
NXP Employee

Hello,

  if the tRPA (PREA) is not provided in DRAM datasheet, one can

set it as tRP or  tRP+1 for assurance.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
882 Views
Yuri
NXP Employee
NXP Employee

Hello,

  if the tRPA (PREA) is not provided in DRAM datasheet, one can

set it as tRP or  tRP+1 for assurance.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
881 Views
ko-hey
Senior Contributor II

Hello Yuri

I understand as follow.

User can set it whichever user like if it not describe in datasheet.

User need test both of parameters, right ?

Ko-hey

0 Kudos
Reply
881 Views
Yuri
NXP Employee
NXP Employee

Yes, users can try both cases : tRPA = tRP and tRPA = tRP+1

~Yuri.

881 Views
ko-hey
Senior Contributor II

OK, thanks.

Ko-hey

0 Kudos
Reply