Waking up board after shutdown by RTC alarm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Waking up board after shutdown by RTC alarm

1,378 Views
pratyushtomar
Contributor IV

I have a custom board based on imx6ul evk. I know it's possible to wake up board from sleep by RTC alarm but is it possible in case of shutdown also? Suppose we set an alarm and shutdown board then can configure our board to wake up by RTC alarm. 

Labels (3)
0 Kudos
Reply
1 Reply

1,099 Views
Yuri
NXP Employee
NXP Employee

Hello,

  According to section 46.2.2.2 (Time counter alarm) of i.MX 6UltraLite  Reference Manual,

Rev. 1, 04/2016 : 
"The SNVS _HP non-secure RTC has its own time alarm register. Any application can
update this register. The SNVS _HP time alarm can generate interrupts to alert the host
processor and can wake up the host processor from one of its low-power modes. Note
that this alarm cannot wake up the entire system if it is powered off because this alarm
would also be powered off."

  As for the SRTC - please refer to i.MX6UL Security Reference Manual. We cannot discuss

this  in public anyway.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply