Wake up IMX6UL from USB host

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wake up IMX6UL from USB host

2,231件の閲覧回数
tuyennguyen
Contributor I

I am using IMX6UL in a customized board. The device works as a USB-powered gadget that receives commands from host using control and bulk transfers. I want to put the device into "suspend" mode for power saving when there is no data activity on DM and DP and wake it up when host initiates some data transaction. I follow "Linux Reference Manual" for Power Management and USB wakeup usage. However it seems that the wake up feature of USB only works when there is external usb device plugged in/out of OTG port. Is there any way that I can wake my device up when it is plugged into a host and there is activity initiated from host without plugging it in/out. Thank you very much!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,000件の閲覧回数
tuyennguyen
Contributor I

Thank you for your reply but I dont see any /sys/bus/usb/devices/usb1/power/wakeup in my kernel. How can I enable it  and is /sys/bus/usb/devices/usb1 is for USB Host? When I call "suspend", the USB gadget (imx6-based device) is automatically unplugged from host. And I have no idea how to wake it up just by DM and DP. And in the document, NXP said that I can wake the device up by VBus and ID pin. Does that mean the device is only wake up when it is in host mode? 

0 件の賞賛
返信

2,000件の閲覧回数
b36401
NXP Employee
NXP Employee

Please try such command:

# echo enabled > /sys/bus/usb/devices/usb1/power/wakeup

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信