Wake up IMX6UL from USB host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wake up IMX6UL from USB host

2,236 Views
tuyennguyen
Contributor I

I am using IMX6UL in a customized board. The device works as a USB-powered gadget that receives commands from host using control and bulk transfers. I want to put the device into "suspend" mode for power saving when there is no data activity on DM and DP and wake it up when host initiates some data transaction. I follow "Linux Reference Manual" for Power Management and USB wakeup usage. However it seems that the wake up feature of USB only works when there is external usb device plugged in/out of OTG port. Is there any way that I can wake my device up when it is plugged into a host and there is activity initiated from host without plugging it in/out. Thank you very much!

Labels (1)
0 Kudos
Reply
2 Replies

2,005 Views
tuyennguyen
Contributor I

Thank you for your reply but I dont see any /sys/bus/usb/devices/usb1/power/wakeup in my kernel. How can I enable it  and is /sys/bus/usb/devices/usb1 is for USB Host? When I call "suspend", the USB gadget (imx6-based device) is automatically unplugged from host. And I have no idea how to wake it up just by DM and DP. And in the document, NXP said that I can wake the device up by VBus and ID pin. Does that mean the device is only wake up when it is in host mode? 

0 Kudos
Reply

2,005 Views
b36401
NXP Employee
NXP Employee

Please try such command:

# echo enabled > /sys/bus/usb/devices/usb1/power/wakeup

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply