WM8960 in Linux BSP L3.0.35

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WM8960 in Linux BSP L3.0.35

1,244件の閲覧回数
geekdarcy
Contributor III
Hi everyone,
 
I'm developing a new board based on the IMX6q.

I'm trying to  port the audio codec WM8960 in Linux BSP L3.0.35.
The result is as follows:
1.png
When I executed the command “aplay   wo.wav   ", it was suspended.I can not hear any sound.
Some debug info is as follows:
2.png
3.png
I'm not very clear principle of  ALSA Soc driver.
Any clue about that error?  Any help , please!
 
Kind regards!
ラベル(2)
0 件の賞賛
返信
1 返信

1,116件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

I apologize for the delay,

Can you please see the below document.

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux Multimedia Codecs Docume...

Probably, that document can help you.

Best Regards,

Diego.

0 件の賞賛
返信