Here i mentioned the wifi low signal connection issue details.
We are using MAYA W166 with IMXRT1064 ,using their SDK application for modem communication. Where we are facing wifi connection issue when the signal strength is -60dbm and above, even though router is available in scan list. SDK 2.11.1 version.
We carried out low signal related test cases in both 2.4GHz and 5GHz band.
- In 5GHz band, the device is unable to connect and communicate with the server at -84 dbm it is flaky and take more then 46 sec.
- In 2.4 GHz the device is unable to connect at -60 dbm signal strength. SDK 2.11.1 version.
For connection test at low signal we config device with wifi router and kept device 6 to 10 meter away from router. with this test setup ,device shows (-60 dbm to -80dbm)signal strength.
In this wifi signal strength range we face below issues
- Device not connect with network within 30 seconds. (-60dbm to -75 dbm)at 2.4Ghz and (-75dbm to -85dbm) at 5Ghz
Some times device able to connect with router but unable to transmit data to server over TCP protocol.With (-60dbm to -75 dbm)at 2.4Ghz and (-75dbm to -85dbm) at 5Ghz try to send sample data to server via TCP protocol this will reproduce the issue what we currently facing