WIFI MODEM ON ULTRALITE SD1 BUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WIFI MODEM ON ULTRALITE SD1 BUS

467 Views
nachodiz
Contributor III

Dear all

We´re Finishing our Schematic and Layout for our new board design

The board will run Linux From eMMC on SD2 Bus

On SD1 Bus i will place a Wifi Modem but also a SD card for fast bsp development (without the wifi modem for BSP development) , the final board will only have the WIFI modem  (Without SD)
On the evk board the SD card is connected to SD2 bus (without mechanical card detect) shared with optional emmc

Can I ommit the MECHANICAL card detect for this SD1 bus when using SD or Wifi modem on this SD1 bus?
I´ve connected it Just In case on the same pin that the EVK ultralite board uses for the SD1 on the Base Board

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply
1 Reply

412 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nacho

you are right, one can omit the MECHANICAL card detect for SD1 bus when using SD or Wifi modem on SD1 bus.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply