Video play failed with gst-launch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video play failed with gst-launch

2,631件の閲覧回数
raybloodworth
Contributor II

I'm trying to play video on MCIMX6Q-SDP, But got some errors.

   log:

   #gst-launch-1.0 playbin uri=file:///opt/test/004.mp4 video-sink=imxeglvivsink

Setting pipeline to PAUSED...

Pipeline is PREROLLING...

Missing element: MPEG-4 AAC decoder

   It seems like there's no MPEG-4 AAC decoder in filesystem.

   Where to find the decoder or how to port it into my filesystem

ラベル(4)
0 件の賞賛
返信
1 返信

1,586件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Freescale AACplus decoder is included in special package.

It is stated in i.MX6 Series Multimedia Release Notes.

Now You may try the next packages :

LTIB :

https://www.freescale.com/webapp/Download?colCode=L3.0.101_4.1.1_AACP_CODECS&appType=license&locatio...

Yocto :

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_AACP_CODECS&appType=license&locatio...

Summary Page :

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信