Video getting cropped

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video getting cropped

1,385件の閲覧回数
ramakrishnakama
Contributor I

Video property is as follows:

Topology:

  container: Quicktime

    audio: MPEG-4 AAC

    video: H.264

 

 

Properties:

  Duration: 0:15:20.810000000

  Seekable: yes

  Tags:

      video codec: H.264 / AVC

      maximum bitrate: 3695752

      bitrate: 749856

      audio codec: MPEG-4 AAC audio

      language code: en

      datetime: "2013-07-05T14:54:42.000000+0530"

      container format: ISO MP4/M4A

 

If we play video using palybin, subtitle not displaying completely. Subtitle is getting cropped.

 

We observed, aiurdemux giving height=502 and vpudec giving height=512 and crop bottom set to 10.

So subtitle in  bottom is getting cropped.

 

Video is uploaded in FTP at path : /data/From_Allgo_To_FSL/video

 

We are using gst-fsl-plugins version 3.5.7 and gstreamer version 10.36

 

Result of "uname -a" is

Linux freescale 3.0.35-2154-g94689e1 #180 SMP PREEMPT Wed Mar 4 15:24:49

CST 2015 armv7l GNU/Linux

 

BSP version is 3.0.35 based customized BSP.

Board is IM6D based customized board .

 

This is very urgent, for a production program. SOP is very close.

Please help us analysing this ASAP.

 

Regards:

Ramakrishna Kamath

Original Attachment has been moved to: video_crop_log.txt.zip

Original Attachment has been moved to: gst_log.txt.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,308件の閲覧回数
jack_mao
NXP Employee
NXP Employee

Hi ramakrishnakamath,

     This is due to hardware limitation, the IPU require 8 pixels  align, so the video was cropped several lines.

best regards

Jack

0 件の賞賛
返信