Verify whether hardware caam is used or not? Android 13

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Verify whether hardware caam is used or not? Android 13

1,122 Views
sibrain-himanshu
Contributor II

We are trying to enable CAAM driver, and wanted to know how to check if hardware crypto is used.

 

Below list of drivers we have enabled.

# CONFIG_CRYPTO_MANAGER_DISABLE_TESTS is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_SM=y

# CONFIG_CRYPTO_DEV_FSL_CAAM_SECVIO=m
# CONFIG_CRYPTO_DEV_FSL_CAAM=m
CONFIG_CRYPTO_DEV_FSL_CAAM_SM_TEST=y
# CONFIG_CRYPTO_DEV_FSL_DPAA2_CAAM=m
CONFIG_CRYPTO_DEV_FSL_CAAM_COMMON=y
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_DEBUG=y
CONFIG_CRYPTO_DEV_FSL_CAAM_JR=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RINGSIZE=9
# CONFIG_CRYPTO_DEV_FSL_CAAM_INTC is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API_QI=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_PKC_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_API=y
CONFIG_CRYPTO_DEV_FSL_DPAA2_CAAM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_TEST=y
 
Interrupt Count before,
 
cat /proc/interrupts | grep jr
68001 0 0 0 GICv3 138 Level 30902000.jr
354478 0 0 0 GICv3 146 Level 30903000.jr
 
Log for tcrypt.ko is added,

 

 

verdin_8mp:/vendor/lib/modules # insmod tcrypt.ko  sec=1 mode=406
[  187.413899][ T2468]
[  187.413899][ T2468] testing speed of async sha512 (sha512-generic)
[  187.422490][ T2468] tcrypt: test  0 (   16 byte blocks,   16 bytes per update,   1 updates):
[  188.420262][ T2468] 604168 opers/sec,   9666688 bytes/sec
[  188.425690][ T2468] tcrypt: test  1 (   64 byte blocks,   16 bytes per update,   4 updates): 449838 opers/sec,  28789632 bytes/sec
[  189.436026][ T2468] tcrypt: test  2 (   64 byte blocks,   64 bytes per update,   1 updates):
[  190.432261][ T2468] 614505 opers/sec,  39328320 bytes/sec
[  190.446214][ T2468] tcrypt: test  3 (  256 byte blocks,   16 bytes per update,  16 updates): 145526 opers/sec,  37254656 bytes/sec
[  191.456017][ T2468] tcrypt: test  4 (  256 byte blocks,   64 bytes per update,   4 updates): 202257 opers/sec,  51777792 bytes/sec
[  192.464024][ T2468] tcrypt: test  5 (  256 byte blocks,  256 bytes per update,   1 updates):
[  193.460263][ T2468] 233653 opers/sec,  59815168 bytes/sec
[  193.474215][ T2468] tcrypt: test  6 ( 1024 byte blocks,   16 bytes per update,  64 updates):
[  194.472281][ T2468]  44219 opers/sec,  45280256 bytes/sec
[  194.477699][ T2468] tcrypt: test  7 ( 1024 byte blocks,  256 bytes per update,   4 updates):  78019 opers/sec,  79891456 bytes/sec
[  195.488035][ T2468] tcrypt: test  8 ( 1024 byte blocks, 1024 bytes per update,   1 updates):
[  196.484272][ T2468]  82465 opers/sec,  84444160 bytes/sec
[  196.498228][ T2468] tcrypt: test  9 ( 2048 byte blocks,   16 bytes per update, 128 updates):  23019 opers/sec,  47142912 bytes/sec
[  197.508048][ T2468] tcrypt: test 10 ( 2048 byte blocks,  256 bytes per update,   8 updates):  41433 opers/sec,  84854784 bytes/sec
[  198.516033][ T2468] tcrypt: test 11 ( 2048 byte blocks, 1024 bytes per update,   2 updates):  43703 opers/sec,  89503744 bytes/sec
[  199.524033][ T2468] tcrypt: test 12 ( 2048 byte blocks, 2048 bytes per update,   1 updates):
[  200.520268][ T2468]  44281 opers/sec,  90687488 bytes/sec
[  200.534217][ T2468] tcrypt: test 13 ( 4096 byte blocks,   16 bytes per update, 256 updates):  11725 opers/sec,  48025600 bytes/sec
[  201.544107][ T2468] tcrypt: test 14 ( 4096 byte blocks,  256 bytes per update,  16 updates):  21411 opers/sec,  87699456 bytes/sec
[  202.552060][ T2468] tcrypt: test 15 ( 4096 byte blocks, 1024 bytes per update,   4 updates):  22626 opers/sec,  92676096 bytes/sec
[  203.560064][ T2468] tcrypt: test 16 ( 4096 byte blocks, 4096 bytes per update,   1 updates):
[  204.556290][ T2468]  22996 opers/sec,  94191616 bytes/sec
[  204.570247][ T2468] tcrypt: test 17 ( 8192 byte blocks,   16 bytes per update, 512 updates):   5916 opers/sec,  48463872 bytes/sec
[  205.580033][ T2468] tcrypt: test 18 ( 8192 byte blocks,  256 bytes per update,  32 updates):  10888 opers/sec,  89194496 bytes/sec
[  206.588046][ T2468] tcrypt: test 19 ( 8192 byte blocks, 1024 bytes per update,   8 updates):  11513 opers/sec,  94314496 bytes/sec
[  207.596107][ T2468] tcrypt: test 20 ( 8192 byte blocks, 4096 bytes per update,   2 updates):  11679 opers/sec,  95674368 bytes/sec
[  208.604087][ T2468] tcrypt: test 21 ( 8192 byte blocks, 8192 bytes per update,   1 updates):
[  209.600282][ T2468]  11694 opers/sec,  95797248 bytes/sec
insmod: failed to load tcrypt.ko: Try again

 

 

 

Interrupt Count After checking tcrypt,

cat /proc/interrupts | grep jr
68461 0 0 0 GICv3 138 Level 30902000.jr
356906 0 0 0 GICv3 146 Level 30903000.jr

 

 

/proc/crypto                                                               <                                                                             name         : authenc(hmac(sha512),cbc(des3_ede))                                                                                                          driver       : authenc(hmac(sha512-generic),cbc-3des-caam)                                                                                                  module       : kernel                                                                                                                                       priority     : 30100                                                                                                                                        refcnt       : 1                                                                                                                                            selftest     : passed                                                                                                                                       internal     : no                                                                                                                                           type         : aead                                                                                                                                         async        : yes                                                                                                                                          blocksize    : 8                                                                                                                                            ivsize       : 8                                                                                                                                            maxauthsize  : 64                                                                                                                                           geniv        : <none>                                                                                                                                                                                                                                                                                                   name         : authenc(hmac(sha512),cbc(des))                                                                                                               driver       : authenc(hmac(sha512-generic),cbc-des-caam)                                                                                                   module       : kernel                                                                                                                                       priority     : 30100                                                                                                                                        refcnt       : 1                                                                                                                                            selftest     : passed                                                                                                                                       internal     : no                                                                                                                                           type         : aead                                                                                                                                         async        : yes                                                                                                                                          blocksize    : 8                                                                                                                                            ivsize       : 8                                                                                                                                            maxauthsize  : 64                                                                                                                                           geniv        : <none>                               

 

 

We are using Android 13 OS.

Please suggest us way to verify whether Hardware caam is used or not.

0 Kudos
Reply
1 Reply

1,100 Views
Harvey021
NXP TechSupport
NXP TechSupport

These info seems show that Hardware caam is used. Can you please tell why you need to enable the caam driver in non-secure? 

 

Regards

Harvey

0 Kudos
Reply