Hello,
Does it mean that it's impossible, or ?
Just for a background, the current visualized pipeline looks like this:
# Start ISP Mediaserver in the background
/opt/imx8-isp/bin/start_isp.sh &
# Start GStreamer pipeline for image transmission via network
gst-launch-1.0 v4l2src device=/dev/video3 \
! video/x-raw,format=YUY2,width=1920,height=1080 \
! vpuenc_hevc \
! rtph265pay \
! udpsink host=192.168.1.2 port=1234
The final application will not utilize GStreamer. Therefore, it is necessary to find an alternative method for passing frames to the VPU. Ideally, the endpoint of the Dewarp Engine can be directly connected to the VPU sink in the device tree.
So how to achieve something like that?
Andy