VPU handtro daemon crashed in custom board using iMX8MP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VPU handtro daemon crashed in custom board using iMX8MP

2,523 次查看
trongthinh
Contributor IV

I have a board configured as follows:
- Chip: iM8MP
- RAM: 4GB
- EMMC: 8GB.
- Audio Codec: TLV320DAC3100IRHBRYocto BSP: https://github.com/nxp-imx/imx-manifest/blob/imx-linux-mickledore/imx-6.1.36-2.1.0.xml


I have successfully brought up the Audio codec and tested it with a wave file.

$ aplay 24_48k_PerfectTest.wav

Playing WAVE '24_48k_PerfectTest.wav' : Signed 24 bit Little Endian in 3bytes, Rate 48000 Hz, Stereo

The sound comes out accurately and clearly. I continued testing using gst-play-1.0, because I wanted to play many other audio formats. I have a problem here. Take a look at the log below.

gst-play-1.0 24_48k_PerfectTest.wav
[   26.593952] audit: type=1701 audit(1672502419.824:18): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=440 comm="vsidaemon" exe="/usr/bin/vsidaemon" sig=6 res=1
[   36.834279] audit: type=1701 audit(1672502430.068:19): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=441 comm="vsidaemon" exe="/usr/bin/vsidaemon" sig=6 res=1
[   37.718446] audit: type=1334 audit(1672502430.952:20): prog-id=10 op=UNLOAD
[   37.725453] audit: type=1334 audit(1672502430.952:21): prog-id=9 op=UNLOAD
Press 'k' to see a list of keyboard shortcuts.
Now playing /home/root/24_48k_PerfectTest.wav
Redistribute latency...
Redistribute latency...
0:00:05.5 / 0:00:13.2

 

/usr/bin/vsidaemon crashed multiple time, and after about one minute the sound is emitted. I would like some suggestions to trouble shoot this problem? I think the correct case should be: vsidaemon doesn't crash and the sound is emitted immediately.

 

 

0 项奖励
回复
6 回复数

2,513 次查看
joanxie
NXP TechSupport
NXP TechSupport

how about gplay-1.0? and pls share your wav file here, let me test again

0 项奖励
回复

2,508 次查看
trongthinh
Contributor IV

I tried gplay-1.0 and got them same problem

gplay-1.0 24_48k_PerfectTest.wav

FSL_GPLAY2_01.00_LINUX build on Aug  4 2023 01:42:29

[   82.101677] audit: type=1701 audit(1672502470.392:20): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=507 comm="vsidaemon" exe="/usr/bin/vsidaemon" sig=6 res=1
[   92.133255] audit: type=1701 audit(1672502480.424:21): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=508 comm="vsidaemon" exe="/usr/bin/vsidaemon" sig=6 res=1
playbin3 is enabled
=========== fsl_player_play() ==================

FSL_GPLAY2_01.00_LINUX build on Aug  4 2023 01:42:29
        [h]display the operation Help
        [p]Play
        [s]Stop
        [e]Seek
        [a]Pause when playing, play when paused
        [v]Volume
        [m]Switch to mute or not
        [>]Play next file
        [<]Play previous file
        [r]Switch to repeated mode or not
        [u]Select the video track
        [d]Select the audio track
        [b]Select the subtitle track
        [n]Select adaptive playback track
        [f]Set full screen
        [z]resize the width and height
        [t]Rotate
        [c]Setting play rate
        [i]Display the metadata
        [x]eXit
State changed: buffering
State changed: playing
[Playing (No Repeated)][Vol=1.0][00:00:00/00:00:13]

I attched my audio file.

0 项奖励
回复

2,464 次查看
joanxie
NXP TechSupport
NXP TechSupport

where do you need get audio? I tested gstreamer command as below, and can get audio from headphone,

when use gplay-1.0, get the message as below, which means gplay uses imxaudioxcvr codec, this codec isn't  supported by current gstreamer, so I use another command to replace

joanxie_0-1704790519183.png

firstly you need use aplay -l to check all of codecs current bsp support

joanxie_1-1704790583809.png

then I used command to test by wm8960 codec as below

gst-launch-1.0 playbin uri=file:///media/24_48k_PerfectTest.wav audio-sink="alsasink device=hw:1,0"

joanxie_2-1704790628203.png

 

 

 

0 项奖励
回复

2,379 次查看
trongthinh
Contributor IV
I have found that the part number of iMX8MP in my custom board is MIMX8ML4CVNKZAB. This part number does not have VPU. So I think this is the reason of VPU hantro daemon crashed.
0 项奖励
回复

2,365 次查看
joanxie
NXP TechSupport
NXP TechSupport

ok, 4 stands for i.MX 8M Plus QuadLite which doesn't have vpu and npu, since you need VPU, pls don't choose this part number

0 项奖励
回复

2,491 次查看
joanxie
NXP TechSupport
NXP TechSupport

let me reproduce this on my side and tell you later

0 项奖励
回复