VPU enable in i.mx8qxp c0 - tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU enable in i.mx8qxp c0 - tool

ソリューションへジャンプ
2,043件の閲覧回数
r_trivedi123
Contributor IV


Hi,

I am working on i.mx8qxpc0 CPU-based custom board.
It is running LF5.10.35_2.0.0 yocto build.

As I have been through the yocto release note for the same BSP and it has GStreamer v4l2h264enc: plugin available, I tried that as well, and check the CPU load, it was 10% only.
However, HD files are taking too much time to get encoded.

Also while using this plugin in the pipeline I tried checking dmesg but was not able to see any logs related to VPU.

I could only see logs while boot up for VPU about the firmware.

My query is how to ensure VPU is being used while encoding?

Is there any tool available?
Are there any driver logs we can enable to verify?
Why HD files are taking longer to get encoded?

Please let me know if any information is required from my side.

Any help would be greatly appreciable.

--

Thanks

タグ(3)
0 件の賞賛
返信
1 解決策
1,922件の閲覧回数
r_trivedi123
Contributor IV

Hi @joanxie ,
Update from my end on VPU,

  1. Run CPU in performance mode

    $ echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
  2. Enable logs to validate VPU usage
    1. echo "7" > /sys/module/vpu_malone/parameters/vpu_dbg_level_decoder
    2. echo "16384" > /sys/module/vpu_windsor/parameters/vpu_dbg_level_encoder
  3. Check encoding/decoding and its dmesg logs to veryfy RPC
    1. gst-launch-1.0 v4l2src device=/dev/video3 io-mode=dmabuf-import ! 'video/x-raw,format=(string)NV12,width=1280,height=720,framerate=(fraction)30/1' ! queue ! v4l2h264enc output-io-mode=dmabuf ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! glimagesink render-rectangle='<0, 0, 1024, 768>' &
  4.  

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,923件の閲覧回数
r_trivedi123
Contributor IV

Hi @joanxie ,
Update from my end on VPU,

  1. Run CPU in performance mode

    $ echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
  2. Enable logs to validate VPU usage
    1. echo "7" > /sys/module/vpu_malone/parameters/vpu_dbg_level_decoder
    2. echo "16384" > /sys/module/vpu_windsor/parameters/vpu_dbg_level_encoder
  3. Check encoding/decoding and its dmesg logs to veryfy RPC
    1. gst-launch-1.0 v4l2src device=/dev/video3 io-mode=dmabuf-import ! 'video/x-raw,format=(string)NV12,width=1280,height=720,framerate=(fraction)30/1' ! queue ! v4l2h264enc output-io-mode=dmabuf ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! glimagesink render-rectangle='<0, 0, 1024, 768>' &
  4.  

 

 

 

0 件の賞賛
返信
2,011件の閲覧回数
r_trivedi123
Contributor IV

Hi,
Can anyone help in here ?

 

Thanks

 

タグ(3)
0 件の賞賛
返信
2,033件の閲覧回数
r_trivedi123
Contributor IV

Hi @joanxie ,
Thanks for the quick replay.

I tried using test utlis as well but then how do i ensure on VPU usage ?

  • Any dmesg log should be checked ?
  • Any gputop ot top alike utitlity available to monitor VPU load ?

Also why might HD file are taking too long to get encoded if hardware VPU is being used ?

--
Thanks

 

 

0 件の賞賛
返信
1,979件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can use the command like below to check vpu:

cat /proc/interrupts | grep vpu

0 件の賞賛
返信
2,018件の閲覧回数
r_trivedi123
Contributor IV

Hi @joanxie ,
Ant debug pointer on above ?

 

Thanks

 

0 件の賞賛
返信
2,036件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

if you just want to test vpu, one can use unit test directly, the path should be imx-test/test/mxc_v4l2_vpu_test

 

0 件の賞賛
返信