Hi,
I am working on i.mx8qxpc0 CPU-based custom board.
It is running LF5.10.35_2.0.0 yocto build.
As I have been through the yocto release note for the same BSP and it has GStreamer v4l2h264enc: plugin available, I tried that as well, and check the CPU load, it was 10% only.
However, HD files are taking too much time to get encoded.
Also while using this plugin in the pipeline I tried checking dmesg but was not able to see any logs related to VPU.
I could only see logs while boot up for VPU about the firmware.
My query is how to ensure VPU is being used while encoding?
Is there any tool available?
Are there any driver logs we can enable to verify?
Why HD files are taking longer to get encoded?
Please let me know if any information is required from my side.
Any help would be greatly appreciable.
--
Thanks
Solved! Go to Solution.
Hi @joanxie ,
Update from my end on VPU,
Hi @joanxie ,
Update from my end on VPU,
Hi @joanxie ,
Thanks for the quick replay.
I tried using test utlis as well but then how do i ensure on VPU usage ?
Also why might HD file are taking too long to get encoded if hardware VPU is being used ?
--
Thanks
you can use the command like below to check vpu:
cat /proc/interrupts | grep vpu
if you just want to test vpu, one can use unit test directly, the path should be imx-test/test/mxc_v4l2_vpu_test