Hello all,
I'm verifying my i.MX6DL custom board that running Android ICS(4.0.4).
I have some questions about the VDD_PU_CAP.
(1) I measured the VDD_PU_CAP. Sometimes, that was drop to approximately 0.2V. Is this correctly?
Operating range of the VDD_PU_CAP is between 1.15V and 1.225V according to the Datasheet (IMX6SDLCEC.pdf : Rev 5).
(2) It looks like overvoltage has occurred when it returns to the normal voltage. Is this cause the software?
(I attached two waveforms.)
Hello,
From Table 2-6 (Power and decouple recommendations) of “Hardware Development
Guide for i.MX 6 …”
’Maximum ripple voltage requirements.
Common requirement for ripple noise should be less than
5% Vp-p of supply voltage average value.
Related power rails affected: all VDD_xxx_IN and VDD_xxx_CAP.
< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >
To avoid issues - please follow recommendations of the Table 2-6.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------