V4L2 Problem on imx8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

V4L2 Problem on imx8QM

ソリューションへジャンプ
5,148件の閲覧回数
CYL
Contributor II

Dear NXP,

We use the L5.4.70_2.3.0_MX8QM Linux release, and follow the guide:https://www.nxp.com.cn/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

then flash to SD Card:sudo dd if=imx-image-multimedia-imx8qmmek.wic of=/dev/sd bs=1M conv=fsync

Using this SDCard, we can boot the linux os. But, when we check the v4l2 function,  Crash occurred.

Details in the attach file : Crash.TXT,  the dmesg.

Any idea or suggestions?

Best regards

0 件の賞賛
返信
1 解決策
5,126件の閲覧回数
CYL
Contributor II

Try to change boot params, works

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,127件の閲覧回数
CYL
Contributor II

Try to change boot params, works

0 件の賞賛
返信
5,068件の閲覧回数
hsaito
Contributor I

Hello, CYL

 

Sorry, forgive a sudden reply. I'm having the same phenomenon.

Would you tell me about change boot params.

 

Best Regards,

0 件の賞賛
返信
5,039件の閲覧回数
CYL
Contributor II

Input below commands in uboot command line:

setenv fdt_file xxxx.dtb(a device tree which include the video-in device, I use the hdmi-in dtb file)

saveenv

boot

 

hope that will take effect for you

5,024件の閲覧回数
hsaito
Contributor I

Thank you for reply.

I will refer to your procedure.

 

Regards,

0 件の賞賛
返信