Utilizing enet qos in Zephyr

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Utilizing enet qos in Zephyr

598件の閲覧回数
jim4604
Contributor I

I'm currently using an i.MX8MP running the Zephyr OS and want to utilize enet qos under this system. The externally connected PHY is a DP83630 using the RMII bus. The DP83630 acts as the master providing a 50MHz clock. The enet qos clock configuration is as follows:

CLOCK_DisableClock(kCLOCK_Enet_Qos);

CLOCK_SetRootMux(kCLOCK_RootEnetAxi, kCLOCK_EnetAxiRootmuxSysPll1Div3);
CLOCK_SetRootDivider(kCLOCK_RootEnetAxi, 1U, 1U);

CLOCK_SetRootMux(kCLOCK_RootEnetQos, kCLOCK_EnetQosRootmuxSysPll2Div20);
CLOCK_SetRootDivider(kCLOCK_RootEnetQos, 1U, 1U);

CLOCK_SetRootMux(kCLOCK_RootEnetQosTimer, kCLOCK_EnetQosTimerRootmuxSysPll2Div10);
CLOCK_SetRootDivider(kCLOCK_RootEnetQosTimer, 1U, 1U);

CLOCK_EnableClock(kCLOCK_Enet_Qos);
When initializing MDIO, the system hangs after calling the ENET_QOS_SetSMI(ENET_QOS_Type *base, uint32_t csrClock_Hz) function. Specifically, it hangs at the line:
base->MAC_MDIO_ADDRESS = ENET_QOS_MAC_MDIO_ADDRESS_CR(crDiv);

It appears that accessing the enet qos registers causes the system to hang. Could this issue be related to an error in the clock configuration?

0 件の賞賛
返信
2 返答(返信)

569件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

In your setup, the best idea would be to probe the MDIO bus, confirm that you have the pull-up in MDIO line, probe that the timing of MDIO and MDC complies with MDIO specification, the PHY address is correct and that the PHY returns a message.

Regards

0 件の賞賛
返信

564件の閲覧回数
jim4604
Contributor I
I'm currently running a dual-system setup with Linux + RTOS. When I load the ENET QoS driver on the Linux side before launching Zephyr, the PHY ID can be read normally, which appears correct. However, if I don't load the driver in Linux, the system freezes.
0 件の賞賛
返信