Util-linux package

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Util-linux package

1,718 次查看
Tanu_1827
Contributor I

Hi,

I am trying to build yocto4.0(Kirkstone) for IMX8DXL.

In which having secure partiton software, util-linux package is included for mapper generation in secure partition.

When i add the util-linux package, secure partition works fine but RTC time and date syncronization is not working as expected.

without the util-linux package date and time is synchronised .

So what internally util-linux package works. is there any dependencies is there? for rtc timer reseting
Do you have any suggestions for this?

0 项奖励
回复
2 回复数

1,706 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Tanu_1827 

 

You can refer to util-linux source.

 

You can see that package use the RTC in hwclock-rtc.c.

 

Best regards.

 

Salas.

0 项奖励
回复

1,679 次查看
Tanu_1827
Contributor I

Hi,

what is the difference between pcf85363 and pcf85263 driver?

Is that compatible for both driver code.

0 项奖励
回复