Using timers on RT1050

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using timers on RT1050

1,882件の閲覧回数
rubensjunior
Contributor IV

Dear friends,

Given the available examples, such as the NXP SDK examples for RT1050 family processors, what are the best examples that use processor timing?

Thank you for your attention, a hug!

Rubens Júnior

1 返信

1,770件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In the SDK library for the MIMXRT1050 board, it has provided a variety of demo projects for the timers in the RT1050, it's helpful for the beginner of RT1050.

Have a great day,
TIC

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------