Using the i.MX53 UART CTS signal for automatic transmission control.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the i.MX53 UART CTS signal for automatic transmission control.

ソリューションへジャンプ
1,048件の閲覧回数
mmichaelis
Contributor I
Can the UART on the i.MX53 use the CTS signal to automatically enable when transmitting and disable at the end of transmission.This would be useful for doing half-duplex RS-485 communications.
ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
847件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mmichaelis

unfortunatey not, i.MX53 UART does not fully support RS485 mode

(in particular direction control), opposite to i.MX6 UART, which supports that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
848件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mmichaelis

unfortunatey not, i.MX53 UART does not fully support RS485 mode

(in particular direction control), opposite to i.MX6 UART, which supports that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信