Using only one ddr3 sdram chip(two byte group) for i.MX6 processors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using only one ddr3 sdram chip(two byte group) for i.MX6 processors

1,373 次查看
tinganho
Contributor I

I'm wondering if it is ok to just use two byte group or one ddr3 IC connected to imx6sl processer? I want to only have 2GB ram for my board and I want to use a single chip for it, instead of 2x1GB.

标记 (2)
0 项奖励
回复
1 回复

1,265 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tingam

yes one can use 16 bit configuration MMDC_MDCTL, DSIZ=0 16-bit data bus,

as two byte group or one ddr3 IC connected to imx6sl processer.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复