Using only one ddr3 sdram chip(two byte group) for i.MX6 processors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using only one ddr3 sdram chip(two byte group) for i.MX6 processors

1,355件の閲覧回数
tinganho
Contributor I

I'm wondering if it is ok to just use two byte group or one ddr3 IC connected to imx6sl processer? I want to only have 2GB ram for my board and I want to use a single chip for it, instead of 2x1GB.

タグ(2)
0 件の賞賛
返信
1 返信

1,247件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tingam

yes one can use 16 bit configuration MMDC_MDCTL, DSIZ=0 16-bit data bus,

as two byte group or one ddr3 IC connected to imx6sl processer.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信