Using libcamera on the i.MX6 ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using libcamera on the i.MX6 ULL

1,438 Views
oneil
Contributor II

I was wondering if anyone has experience using libcamera on the i.MX6 ULL and could give some tips on configuring it to work on this device. I'm new to the i.MX6 ULL family as well as libcamera so am not sure where to start.

Per the libcamera FAQs, there is not official support for the i.MX6 ULL. However, this post on NXP Community suggests that it is possible to use it.

Any help is appreciated.

Tags (1)
0 Kudos
Reply
1 Reply

1,423 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @oneil 

If you are using NXP yocto project and NXP demo images, you can check if there is gstreamer libcamera libray in /usr.