Using libcamera on the i.MX6 ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using libcamera on the i.MX6 ULL

1,426件の閲覧回数
oneil
Contributor II

I was wondering if anyone has experience using libcamera on the i.MX6 ULL and could give some tips on configuring it to work on this device. I'm new to the i.MX6 ULL family as well as libcamera so am not sure where to start.

Per the libcamera FAQs, there is not official support for the i.MX6 ULL. However, this post on NXP Community suggests that it is possible to use it.

Any help is appreciated.

タグ(1)
0 件の賞賛
返信
1 返信

1,411件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @oneil 

If you are using NXP yocto project and NXP demo images, you can check if there is gstreamer libcamera libray in /usr.