Using external RTC from SCFW in IMX8QXP based board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using external RTC from SCFW in IMX8QXP based board

1,871 Views
_asif_muhammed_
Contributor III

Hi,

I have an external RTC on my custom board, which is connected to the SCU I2C. Could someone please confirm whether I can use it or not from SCFW?

Will I be only able to use the SNVS RTC from SCFW?

Will there be any internal driver which can communicate to an external RTC? Could someone please point me in the right direction?

@kerryzhou 

0 Kudos
Reply
2 Replies

1,850 Views
_asif_muhammed_
Contributor III

Thank you Bio_TICFSL.I have gone through the document. It seems that it is an internal RTC of SNVS.

Is it possible to interface an external RTC to the SCU via the SCU_I2C?

0 Kudos
Reply

1,855 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Should it be SC_R_SNVS (since that's where the RTC is located).  Please check it:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Timer-ser...

 

Regards

0 Kudos
Reply