Using a P&E Micro Universal Multilink probe on the MIMXRT1010-EVK.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using a P&E Micro Universal Multilink probe on the MIMXRT1010-EVK.

923 次查看
JimDon
Senior Contributor III

To use the P&E Multilink on the MIMXRT1010-EVK.:

Connect the 10 pin cable from the probe  to connector  J55 - red side with pin1

Disconnect the USB connector from J42 and connect to J9, Move the Jump on J1 from 1-2 to 3-4.

SW8 OFF-OFF-ON-OFF ( this is the default)

0 项奖励
回复
0 回复数