Using WBZ450UE Thread Module with i.MX95 Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using WBZ450UE Thread Module with i.MX95 Processor

1,281 Views
Ankit_chauhan
Contributor I

Hello there,

I am working with the i.MX95 processor and looking to integrate the WBZ450UE Thread module. I have a few questions:

1. Can we directly use the WBZ450UE module with the i.MX95 processor?

2. If yes, what are the key requirements for interfacing the module with the i.MX95? (e.g., drivers, firmware support, etc.)

3. Is there any existing software stack or example available for integrating the WBZ450UE with Linux (Yocto-based)?

 

Any guidance on hardware and software integration would be greatly appreciated.

Thanks!

0 Kudos
Reply
2 Replies

1,252 Views
ericda
Contributor II

Check IW612 here for more information, hope it helps!

1,268 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Ankit_chauhan!

Thank you for contacting NXP Support!

 

Unfortunately we don't have the drivers for that BLE module integrated in our BSP.

 

I recommend to use the IW612 instead, that wifi/ble module is already working with the iMX95 processor.

 

Best Regards!

Chavira

0 Kudos
Reply