Using SRC_BOOT_CFGx pins as GPIOs?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using SRC_BOOT_CFGx pins as GPIOs?

1,825 次查看
emilzachariageo
Contributor II

Hi Team,

Can we use the SRC_BOOT_CFGx pins as GPIO pins or some SPI dedicated pin?

Are they sampled only during the boot time?

If so, is it okay if we provide the required pull-ups and pull-downs to these pins to set required boot option?

Thanks in advance.

Emil

标签 (2)
0 项奖励
回复
2 回复数

1,771 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Emil

yes this is possible, one can look on sect.2.3 Bus isolation circuit

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,771 次查看
emilzachariageo
Contributor II

Hello Igor,

Thanks.

Warm Regards.

Emil Zacharia George | Senior Hardware Design Engineer

*Mob: +91 **9061665533 *| Skype: emilgeorge93

0 项奖励
回复