Using SRC_BOOT_CFGx pins as GPIOs?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using SRC_BOOT_CFGx pins as GPIOs?

1,876件の閲覧回数
emilzachariageo
Contributor II

Hi Team,

Can we use the SRC_BOOT_CFGx pins as GPIO pins or some SPI dedicated pin?

Are they sampled only during the boot time?

If so, is it okay if we provide the required pull-ups and pull-downs to these pins to set required boot option?

Thanks in advance.

Emil

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,822件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Emil

yes this is possible, one can look on sect.2.3 Bus isolation circuit

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,822件の閲覧回数
emilzachariageo
Contributor II

Hello Igor,

Thanks.

Warm Regards.

Emil Zacharia George | Senior Hardware Design Engineer

*Mob: +91 **9061665533 *| Skype: emilgeorge93

0 件の賞賛
返信