Use pmic touch screen da9063 with imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use pmic touch screen da9063 with imx6

1,676 Views
emmanuelperea
Contributor III

Hello,

I'm using a digi connectcore6 board with an imx6 quad. The Connectcore6 has a da9063 pmic. I want to use the da9063 touch screen module but I don't have the kernel driver for this.

Can anyone help me.

Labels (3)
0 Kudos
Reply
1 Reply

1,546 Views
reyes
NXP TechSupport
NXP TechSupport

Hello,

I’m afraid that since DA9063 is not a PMIC from NXP and also because Connectcore6 board was not developed by NXP, we at NXP are not able to provide support for your question, I recommend you to contact digi and/or Dialog Semiconductor for support.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply