hello everyone:
I use
$ bitbake meta-toolchain
in tmp/deploy/sdk/ have poky-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-1.7.sh
and
$ sh poky-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-1.7.sh
[sudo] password for daiane:
Enter target directory for SDK (default: /opt/poky/1.4.1):
You are about to install the SDK to "/opt/poky/1.4.1". Proceed[Y/n]?y
Extracting SDK...done
Setting it up...done
SDK has been successfully set up and is ready to be used.
but I use
$ arm-poky-linux-gnueabi-gcc hello.c -o hello
In file included from /opt/poky/1.7/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/features.h:389:0,
from /opt/poky/1.7/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/stdio.h:27,
from hello.c:8:
/opt/poky/1.7/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/gnu/stubs.h:7:29: fatal error: gnu/stubs-soft.h: No such file or directory
# include <gnu/stubs-soft.h>
^
compilation terminated.
Can someone please help me to resolve this?
Thanks
解決済! 解決策の投稿を見る。
I checked your command.
It seems you forgot to add "$" before CC.
it is "$CC" not just "CC".
if I use the CC
lxh@lxh-PC:~/lianxi$ CC hello.c
Fatal Python error: Py_Initialize: Unable to get the locale encoding
ImportError: No module named 'encodings'
已放弃 (核心已转储)
poky-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-1.7.sh is installation script to install the toolchain.
Once you have finished the installation by default settings, you will find toolchain located in /opt/poky/1.7
source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi
$CC -o hello hello.c
file hello
hello: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.32, BuildID[sha1]=9c5d95682844a03a2c5563a73184fa142035a1d5, not stripped
Thanks for the response. but
lxh@lxh-PC:~/lianxi$ source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi
lxh@lxh-PC:~/lianxi$ CC -o hello hello.c
Fatal Python error: Py_Initialize: Unable to get the locale encoding
ImportError: No module named 'encodings'
已放弃 (核心已转储)
I checked your command.
It seems you forgot to add "$" before CC.
it is "$CC" not just "CC".
thank you very much!!!
if I use
$ source poky-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-1.7.sh
source: poky-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-1.7.sh: 无法执行二进制文件