Use mcuxpress IDE BSP in GHS IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use mcuxpress IDE BSP in GHS IDE

887 Views
Pavan_Moody
Contributor II

Hi Team,  iam using mmimxrt1170 EVKB Board so i wanted to import BSP of mcuxpress ide so i have seen some provision for ghs in the ide.

is it do able?

if yes, how can we.

0 Kudos
Reply
3 Replies

864 Views
jim65richards
Contributor I

Yes, it is doable. While MCUXpresso IDE is primarily designed for the GNU toolchain, NXP provides a GHS (Green Hills Software) project export feature within the SDK.

To do this, you must first go to the NXP SDK Builder and specifically select the "Green Hills" toolchain option when building/downloading your SDK for the i.MX RT1170. Once downloaded, you can import the SDK into MCUXpresso IDE. To generate the GHS-specific project files, you would typically use the "Export" wizard or use the standalone Project Generator tool found within the SDK's tools folder to create the .gpj files required for the Green Hills MULTI IDE.

0 Kudos
Reply

857 Views
Pavan_Moody
Contributor II
jim65richards,

https://mcuxpresso.nxp.com/select/toolchains i have opened SDK builder but i not able to find ghs tool chain, can you tell me i am following same.
0 Kudos
Reply

842 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Pavan_Moody,

MCUXpresso does not have compatibility with GHS toolchain, only the ones that you have seen on the SDK builder. If you want to use the RT1170 with GHS, I suggest you contact Green Hills for more information on the BSP for the RT1170 on their IDE instead.

BR,
Edwin.

0 Kudos
Reply