Use iMX8M Plus as USB Gadget

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use iMX8M Plus as USB Gadget

1,145件の閲覧回数
swapnilturambekar
Contributor I

Hi,

I am working on iMX8M plus custom board and I want to use this board as gadget to access the stored data. I am able to detect the device on GUI as gadget and can see the data available in the eMMC. But every time I need to restart/reboot the device while creating/deleting the new file. what should I do to reflect the changes at run time.

E.g.

1. Run Gadget mode

2. Create new file say "test.txt" using command line and save it.

3. unable to see the file at GUI.

4. Reboot the device. and run the gadget mode.

5. now able to see the "test.txt" file in GUI.

can anyone face this issue earlier and have idea what need to be done.

Thanks

ラベル(3)
0 件の賞賛
返信
0 返答(返信)