Use iMX8M Plus as USB Gadget

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use iMX8M Plus as USB Gadget

1,152 Views
swapnilturambekar
Contributor I

Hi,

I am working on iMX8M plus custom board and I want to use this board as gadget to access the stored data. I am able to detect the device on GUI as gadget and can see the data available in the eMMC. But every time I need to restart/reboot the device while creating/deleting the new file. what should I do to reflect the changes at run time.

E.g.

1. Run Gadget mode

2. Create new file say "test.txt" using command line and save it.

3. unable to see the file at GUI.

4. Reboot the device. and run the gadget mode.

5. now able to see the "test.txt" file in GUI.

can anyone face this issue earlier and have idea what need to be done.

Thanks

0 Kudos
Reply
0 Replies