Update uImage on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update uImage on iMX6

2,087 Views
giorgiofantin
Contributor I

Hi community,

  i have a big problem (for me),becouse i need to update uImage on my Qt iMX6 while the system is running on MMC. I have a Q7 module, ehere i loaeded u-boot, uImage and FS on the MMC. During the loading, oi copied the wrong uImage and now i have the necessity to update it with the right one.

Is it possible?

I hope that someone helps me

Thanks

Labels (1)
0 Kudos
Reply
2 Replies

1,928 Views
giorgiofantin
Contributor I

The fact is that the kernel loaded first time, has no support for cifs, anche the update got it

No, should be ok, add cifs to the actual kernel loaded

0 Kudos
Reply

1,928 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

To update your image you can try to use mfgtool.

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

It provides the possibility to update the eMMC with a different image.

Best Regards,

Alejandro

0 Kudos
Reply