Unlock RNG with cst 2.3.2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unlock RNG with cst 2.3.2?

1,458 Views
colinhelliwell
Contributor III

Could I get confirmation please about having:

[Unlock]
Engine = CAAM
Features = RNG

in the csf file. AN4581 says that this is included by default on CST v2.3+, but I've also read that it in fact is still needed (when wanting to use this one of the two options).

Just wanted to double-check please. And does it only matter if encryption is being used?

Labels (1)
0 Kudos
Reply
1 Reply

1,330 Views
joanxie
NXP TechSupport
NXP TechSupport

 one can refer to the document as below:

https://community.nxp.com/docs/DOC-330622 

it seems you should add them to the u-boot.csf

0 Kudos
Reply