Unit_tests porting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unit_tests porting

Jump to solution
3,293 Views
xu_ji1
Contributor V

Hi,

I want to porting the unit_tests module that in Yocto project to Android project.

Does it feasible? Please give guide.

Thanks

0 Kudos
Reply
1 Solution
3,168 Views
xu_ji1
Contributor V

What is the scratch?If I porting one module of Unit_tests like camera,is it ok?

Thanks

View solution in original post

0 Kudos
Reply
5 Replies
3,168 Views
art
NXP Employee
NXP Employee

There seems to be no way to directly port the unit_tests application from Linux to Android. A new Android application should be created from the scratch.

Best Regards,
Artur

0 Kudos
Reply
3,169 Views
xu_ji1
Contributor V

What is the scratch?If I porting one module of Unit_tests like camera,is it ok?

Thanks

0 Kudos
Reply
3,168 Views
art
NXP Employee
NXP Employee

Yes, it's OK.

0 Kudos
Reply
3,168 Views
xu_ji1
Contributor V

What is the scratch?

0 Kudos
Reply
3,168 Views
art
NXP Employee
NXP Employee

"From the scratch" is the idiomatic phrase that means "from the very beginning stage".

0 Kudos
Reply