Unexpected SPI frequency variation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unexpected SPI frequency variation

1,347件の閲覧回数
deven_solanki
Contributor III

Hi,

I am working in imx7d sabresd. Right now I am testing SPI which is available in mikrobus with spitest application (link: https://raw.githubusercontent.com/raspberrypi/linux/rpi-3.10.y/Documentation/spi/spidev_test.c).

I am changing frequency (from application) so mostly I am getting nearby clock value(like for 25MHz output frequency is 20MHz), that is ok because it is using divider.

But when I am giving 3MHz,4MHz,8MHz and 9MHz I am getting very low frequency(below 1MHz), and when I am giving 2MHz it is reflecting as same 2Mhz. Why it is like that?

Thanks in advance,

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,268件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Deven,

which BSP/kernel are you using?

Carlos

0 件の賞賛
返信