Understanding performance for Go-point demos

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Understanding performance for Go-point demos

878件の閲覧回数
ashwanipal01
Contributor I

Please help me with the following Question related to the expected performance of detection models like Mobilenetssdv2:

  1. I am currently following the GitHub Link for understanding the performance of the detection models used in the Go point demo on my IMX8MP hardware. Click here
  2. I could understand that the demonstrations are only for <=480P quality videos.
  3. Is there any sample in which IMX8MP can reach a greater than 20FPS for higher video resolution, like 720p and 1080p. Please share
  4. I am assuming that this hardware can only achieve 20 FPS for <=480P videos for a detection model like mobilenetssdv2. Please suggest if you have any information on this.
  5. BSP version is 5.15.52 krikstone

Thanks 

0 件の賞賛
返信
1 返信

853件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @ashwanipal01!

Thank you for reaching out to NXP Support!

 

The i.MX8MP is capable of supporting 4K resolution at 30fps.

 

It’s possible that the NPU is not being utilized for inference tasks in your current setup. Please ensure that the NPU is properly enabled and integrated into your pipeline to achieve optimal performance.

 

Best regards,
Chavira

0 件の賞賛
返信