Under the Linux3.0.35 kernel version, how to increase the access frequencies of IMX6Q SPI's CS ? The attachment is the picture of SPI access frequencies when clock cycles is 20 MHZ. Red one is CS singal,the yellow one is SPI clock signal.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Under the Linux3.0.35 kernel version, how to increase the access frequencies of IMX6Q SPI's CS ? The attachment is the picture of SPI access frequencies when clock cycles is 20 MHZ. Red one is CS singal,the yellow one is SPI clock signal.

3,100件の閲覧回数
ferdi
Contributor I

Hi :

Under the Linux3.0.35 kernel version, how to increase the access frequencies of IMX6Q SPI's CS ? The attachment is the picture of SPI access frequencies when clock cycles is 20 MHZ. Red one is CS singal,the yellow one is SPI clock signal.

Ferdi

Best Regards!

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,930件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ferdi

one can try to enable dma:

https://community.freescale.com/thread/328465

https://lkml.org/lkml/2014/9/15/1075

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,930件の閲覧回数
ferdi
Contributor I

Dear igorpadykov:

     The connection patch is based on the IMX51 platform, which is not compatible with the IMX6Q platform, Do not know if there is a Linux3.0.35 based IMX6Q patch platform? Thank you!

Best regards!

Ferdi

0 件の賞賛
返信