Many people faces with problem on i.MX processors because not well qualified or they confused by documentation where you can set fuses and lock them later. Will be featured processor support this feature for unblow fuses, like SRK hashes, which will be programmed incorrectly or for development purpose?
Hi Maxim
unfortunately it is not possible to "unblow" fuses since
they are "one-time programmable" :
Programmable read-only memory - Wikipedia
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I asked about processors in the future which can support non-OTP like eMMC boot partition switch. It can be overwritten multiple times. But after locking this fuse it will be not possible anymore.
There is for me left only two questions between OTP and non-OTP:
1. Are there any security vulnerabilities?
2. Is it more expensive to implement?