Unable to enable the bluetooth module for Imx8 board (timeout)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to enable the bluetooth module for Imx8 board (timeout)

Jump to solution
3,715 Views
hlatafat
Contributor II

I am using the NXP evaluation board IMX 8MPLUS with combined wifi and bluetooth Azureware chip (AW-CM276MA PUR) . I am having trouble enabling the Bluetooth module.

I followed the instruction from the document: “UM11483 Getting Started with NXP Wireless Modules for i.MX 8M-Quad Platforms”.

I could successfully enable the wireless module. But for the Bluetooth, first I execute a command “hciattach /dev/ttymxc2 any 115200 flow” as suggested in the document and the result is as expected:

Setting TTY to N_HCI line discipline 

Device setup complete

After that I run the command “hciconfig hci0 up” but with timeout errors:

[ 132.478107] Bluetooth: hci0: command 0x1003 tx timeout 

[ 134.494103] Bluetooth: hci0: command 0x1001 tx timeout

[ 136.510105] Bluetooth: hci0: command 0x1009 tx timeout

Can't init device hci0: Connection timed out (110)

I read manuals very carefully, searched the nxp community and did whatever I could think of without success. Could you please help me solve this problem?

Thank you in advance

0 Kudos
Reply
1 Solution
3,699 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The uart used by  bluetooth is different between i.MX8MP and i.MX8MQ, you can try /dev/ttymxc0

View solution in original post

0 Kudos
Reply
2 Replies
3,700 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The uart used by  bluetooth is different between i.MX8MP and i.MX8MQ, you can try /dev/ttymxc0

0 Kudos
Reply
3,694 Views
hlatafat
Contributor II

Thanks a lot Qmiller.

That solved my problem.

0 Kudos
Reply