UUU tool stops while in flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UUU tool stops while in flashing

3,424 次查看
yibhan
Contributor III

Hi guy,

I have a problem when flash image to the device which is my custom board, but while setuping the device, uuu tools stops and doesn't continue to go forward and error is below in uuu tools:

1:1  1/1[======100%====================] SDP: boot -f u-boot-dtb

1:2 19/19 [Bulk(R): LIBUSB_ERROR_TIMEOUT] FB: ucmd echo "acm..."

I have no idea that error come from. Coudl you please guild me to check some points?

标签 (3)
0 项奖励
回复
1 回复

3,321 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yibeom

for libusb one can check uuu tool requirements

https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.135/UUU.pdf

Also for custom board may be recommended to check usb schematic using

IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复