USB2 host in u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB2 host in u-boot

1,483件の閲覧回数
pyraohms
Contributor III

We are trying to find our modem that is connected to USB2 on our custom imx6ull board. The USB block gets power since we are booting from MFGtool to get into u-boot. But the modem can not be found when running the usb start command. The board is based around the EVK and out u-boot is based around the EVK config.

Does the second USB port needs to be configured from default to support host mode?

Thanks

0 件の賞賛
返信
1 返信

1,396件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Per

one can check if signal usb_id is low. Is modem working fine with usb1.

Also modems may consume much current, one can try to test with usb stick.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信