USB wake support on iMX8QXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB wake support on iMX8QXP

1,889 Views
jith
Contributor II

Hi,

We are using L4.14.98GA BSP on our iMX8QXP platform. We are testing the wakeup features.

As mentioned in Linux user guide,we are able to wake the system from low power mode using debug UART.

Now we are trying with usb wake features by following i.MX Linux Reference Manual, Rev. L4.14.98-2.0.0_ga, 04/2019.But not able to wake the system from low power mode.

Does  L4.14.98GA BSP support USB wakeup feature?

0 Kudos
Reply
1 Reply

1,709 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Jith,

I’m afraid that i.MX8X family is still on preproduction, and we cannot provide additional information or support through this channel yet. In case of requiring help about i.MX8X, please directly contact with your NXP FAE, Sales or DBM.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply