USB type-C (Flashing port) change to USB 3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB type-C (Flashing port) change to USB 3.0

1,039 Views
Jimmychea
Contributor III

Hi.

I will change the i.MX8M Plus evk's USB type-C (flashing port) to USB 3.0. Any software need to change/modify, please provide steps on it? If change to USB 3.0, the UUU flashing tool still able to use ? Thanks 

0 Kudos
Reply
4 Replies

1,020 Views
joanxie
NXP TechSupport
NXP TechSupport

do you mean usb 3.0 port 1? this is usb 3.0 dual role port, you can use it for downloading without change SW, for HW design, pls refer to the Table 30. i.MX 8M Plus USB strapping recommendations and chapter 3.7 USB connectivity of Hardware design guide

0 Kudos
Reply

1,010 Views
Jimmychea
Contributor III

Yup, USB type-C (Port 1). Because i will change it to USB type-A 3.0, so may i know what is the software changes needed and will it impact the image flashing via UUU tool ? Thanks

0 Kudos
Reply

991 Views
joanxie
NXP TechSupport
NXP TechSupport

don't need change software

0 Kudos
Reply

988 Views
Jimmychea
Contributor III

For software part, require to remove the USB type-C configuration on u-boot and also the DTS file. Am i correct ?

0 Kudos
Reply