USB not recognized on iMX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB not recognized on iMX6Q

2,425 次查看
riteshpatel
Contributor II

Hi, 

I have designed Hardware around iMX6Q processor for my project.

I have tested all power rails on the processor and it is successfully up. Now I am trying to connect iMX6 (by setting Boot mode as Serial download mode) USB OTG port with PC USB port to download the U-boot binary. 

I am checking the USB device detection in an MFG tool2.exe from NXP. But It gives me error as "USB not recognized on screen".

I checked in PC device manager and it shows "Unknown USB device (Device Descriptor Request Failed).

Would greatly appreciate an early response.

Thanks & Regards,

Ritesh

标签 (2)
标记 (3)
0 项奖励
回复
2 回复数

2,092 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Ritesh,

I need to inform you that MFG Tool it is only supported by Windows 7 .  If you are having problems detecting the USB can be related to the Windows HOST, we have seen this error before in Windows 8 and Windows 10 since the tool it is not supported because the driver it is not Certified by windows.

Merry Christmas and Happy new Year.

0 项奖励
回复

2,092 次查看
riteshpatel
Contributor II

Hi James

Thanks for the quick response.

I have checked my Hardware on Windows 7 and iMX6Q USB OTG port detected as a device properly. 

Happy New Year.

0 项奖励
回复