USB driver for Windows 10 support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB driver for Windows 10 support

2,304件の閲覧回数
JK-IMX
Contributor V

Hi i.MX champ

Can you please let us know if the USB driver of i.MX 8M would be available for Windows 10 Host PC interface? If yes, How to get the driver installable.

This is not a request regarding USB to UART bridge device driver such like Silab CP210x.

The customer wants to get connected of device btw IMX8' USB port to Windows 10 PC to transfer Camera Stream data in USB3.0 super speed mode.

Thanks.

Regards, 

Arrow

ラベル(1)
0 件の賞賛
返信
1 返信

2,295件の閲覧回数
pete_sensoray
Contributor II

Look for the UVC gadget driver in the Linux kernel source code, specifically drivers/usb/gadget/legacy/webcam.c and drivers/usb/gadget/function/f_uvc.c.  For more info see here: https://docs.kernel.org/usb/gadget-testing.html#uvc-function