USB connection error on MCIMX6Q-SDB Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB connection error on MCIMX6Q-SDB Linux

1,865 Views
YoshihisaSaitou
Contributor I

Hi,

I'm using a MCIMX6Q-SDB board with linux.

When a USB device was connected, the following errors had occurred.

What does this error code mean? (Error-71,Error -18)

 

Example of error messages

- IsoErr: index (6) frame (0) len (137) Error (-71) -

- IsoErr: index (8) frame (0) len (0) Error (-18) -

Thanks.

Labels (3)
0 Kudos
Reply
2 Replies

1,723 Views
YoshihisaSaitou
Contributor I

Hi igor-san,

Thank you for your quick reply.
I will check to see its contents.

Best regards,
Yoshihisa.

0 Kudos
Reply

1,723 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yoshihisa

seems these errors are linux errors described in errno.h,
linux/Documentation/usb/error-codes.txt. One can try to debug

it in drivers/usb using AN4553 Using Open Source Debugging Tools

for Linux on i.MX Processors

http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply